Sensor Open Systems Architecture

Sensor Open Systems Architecture

SOSA™ defines an architecture and standards for modular entities for composing sensors with Electro-Optical/Infrared (EO/IR), Electronic Warfare (EW), Radar, and Signals Intelligence (SIGINT) modalities. Rather than defining an entirely new system, this Standard defines a set of logical modules that group functions, behaviors, and interfaces, which together define the logical architecture of a sensor. As a result, SOSA™ technologies can:

  • Integrate into new or existing systems using SOSA™ defined sensors.
  • Allow for greater design modularity for hardware or software in embedded systems.
  • Permit the user to reconfigure Standards such as OpenVPX™ and SAE AS6169 for use as SOSA™ sensors.
  • Facilitate rapid fielding of embedded technologies and platform reconfiguration.

SOSA Brochure

SOSA Aligned Interconnect Solutions

Download PDF
sosa logo

Mezzanine

While offering greater flexibility as to how a user can interface with a carrier board, SOSA™ makes extensive use of proven and next-gen mezzanine Standards. This allows for high-density data I/O transfer across the full channel, ensuring reliable signal integrity in a rugged form factor.

Current Mezzanine Standards that are featured in SOSA™ include:

  • VITA 42 – supports SOSA™ I/O Intensive Slot Profiles
  • VITA 57.1 – ideal for SOSA™ users prototyping with FPGAs
  • VITA 57.4 – next-gen speeds up to 32 Gbps for FPGA system-use or benchtop work
  • VITA 88 – next-gen mezzanine interconnects allowing for PCIe® 5.0+ speeds and footprint compatibility with VITA 42

xmc logo xmc plus logo fmc logo fmcplus logo

Small Form Factor

As the first Small Form Factor architecture of SOSA™, VITA 74 VNX is a truly modular Standard offering flexibility to integrate SOSA™ sensors in everything from a mesh-network of distributed SBCs to a traditional rackmount system.

Expanding on ANSI/VITA 74.0, SOSA™ VNX Plug-In Cards will utilize a variety of predefined combinations of high-speed, optical, and coaxial connectors. This greatly improves external I/O while allowing for integration of optical and coaxial connectivity in existing VNX systems.

SOSA™ VNX allows for:

  • Addressing the industry need for rugged, high-density solutions in spaces smaller than 3U.
  • Higher density and performance in a package about 33% the size of 3U VPX.
  • Design flexibility ranging from 1x SBC, 8x VNX Plug-In Cards to mesh topologies via cable.
  • Improved two-level maintenance at the box level; no need to replace individual Plug-In Cards.
  • Cost-effective SFF solutions based around COTS modules and connectors.

vnx logo

SOSA Standards

For questions regarding the SOSA™ family of Standards and additional information, please contact us at:

CONTACT SALES

First Name
Last Name
Email
Company
Industry
Estimate Annual Usage
Family
Message

Don't want to fill out a form?
Chat with a product expert directly.

.
.
Designers frequently ask how much gold plating they should specify on the connector pins. As I write this blog, (and yes, I’m old-fashioned and am actually typing it; I’m not using […] The post Gold Plating On Connectors: How Much Do I Need? appeared first on The Samtec Blog....
Samtec Harrisburg attended the 17th annual Penn State Harrisburg Signal/Power Integrity Symposium and MASH Forum on Friday, April 19th 2024, hosted by the Center for Signal Integrity. The main goal of the […] The post Samtec Design Center Attends Annual Penn State Harrisburg SI/P...
As the world gears up to celebrate the 150th running of the Kentucky Derby,the excitement is intense. This iconic event isn’t just about horse racing;it’s a celebration of tradition, athleticism, […] The post Celebrating Community and Innovation: Samtec’s Connection to the 150th ...
Wait . . . An AI hardware platform without a GPU? Is that even possible? Obviuolsy, I jest. GPUs are the workhorse solutions for ever larger LLMs and cutting-edge generative […] The post New AMD Versal AI Edge SoM and Carrier Card From Avnet Feature Samtec Interconnects appeared ...
Artificial Intelligence. Or, the intelligence of computers. It’s all around us, but I think it’s important to remember that this intelligence is driven by human intelligence. It’s the human innovation behind […] The post Artificial Intelligence: How to Manage High Amounts of Dat...