Webinar: Precision RF Connector PCB Launches for 224 Gbps Devices

Presented by: Sandeep Sankararaman The signal-to-noise ratio (SNR) at the input of a device is a critical factor in determining its performance. As the bandwidth of devices approach 100 GHz, it becomes very hard to maintain adequate levels of SNR across the full bandwidth. Connector launches also become increasingly challenging. This gEEk® spEEk webinar aims to demystify the principles behind the design of millimeter wave RF launches. The impact of different design features on stripline launches will be examined and practical approaches to getting the maximum performance will be explained.