JIIA, CoaxPress Standards

Japan Industrial Imaging Association (JIIA) is a Japan-based organization leading technological innovation of industrial imaging. JIIA promotes a global community for organizations related to industrial imaging, thus contributing to the development of industrial imaging standards and products worldwide.

As Japanese industrial imaging companies cover a wide range of the market, JIIA is uniquely positioned to act as a leading developer of industrial imaging technologies. Such categories include industrial cameras, input devices, image processors, image processing software, optical instruments, lighting equipment, and measurement and analysis machinery.

 

CoaXPress 2.0

CoaXPress (CXP) is the world’s leading standard for high-speed imaging in professional and industrial imaging applications such as machine vision, medical imaging, life sciences, broadcast and defense.

CoaXPress is an interface to connect cameras to frame grabbers. It combines the simplicity of coaxial cable with state of the art high speed serial data technology, allowing up to 12.5 Gbps data rate per cable, plus device control and power in the same cable.

CoaXPress is a point-to-point scalable interface. The physical medium between the camera and frame grabber is 75 Ω coaxial cable.

Samtec has a large variety of compliant CoaXPress 2.0 HD-BNC 75Ω connectors and components.

CoaXPress Logo
HDBNC RF
HDBNC RF Cable

CoaXPress Optical Interface

In order to supplement the existing Standard, JIIA has defined Optical Interface guidelines utilizing an optical media interface to communicate between the Device and Host via existing protocols. Samtec addresses this need by means of a custom ECUO FireFly™ module acting as the interconnect solution between the electrical module and optic-receptacle adaptor.

ECUO FireFly

CONTACT SALES

First Name
Last Name
Email
Company
Industry
Estimate Annual Usage
Family
Message

Don't want to fill out a form?
Chat with a product expert directly.

.