Immersion Cooling

Immersion Cooling

Immersion cooling is the process of immersing electronic hardware in a non-conductive liquid such as Engineered Fluids Electrocool or 3M Fluorinert FC-43. Data Centers are among the largest users of immersion cooling to lower their overall energy consumption.

As computing power continues to increase, so does the need to remove heat from those computing systems. The traditional method of using fans is loud, and it also loses efficiency as the ambient temperature increases. Immersion cooling eliminates the need for fans and heat sinks, and offers a more energy efficient method of cooling while eliminating the noise from fans.

Industries and Applications

Testing Specifications

Samtec Interconnects are used in a variety of industries and are used in many different environments. Because of this, Samtec has introduced testing its connectors for immersion cooling applications in addition to the standard qualification testing that interconnect systems are tested towards.

Additional Tests Included for Immersion Cooling Applications:

  • Mating/Unmating/Durability (Humidity, LLCR, Thermal Age and Thermal Shock)
  • Insulation Resistance/Dielectric Withstanding Voltage (IR/DWV)
  • Current Carrying Capacity
  • Current Cycling

Immersion Cooling Qualified Products

Samtec is currently testing all product series below according to demand in Engineered Fluids Electrocool.

SEARAY™ 1.27 mm Pitch
High-Density Arrays
HSB2B
SEAM / SEAF View Report
mPOWER® 2.00 mm Pitch
Ultra Micro Power Connectors
UMPX
UMPT / UMPS View Report
Edge Rate® 0.80 mm Pitch
Rugged High-Speed Strips
ERX8
ERM8 / ERF8 View Report
EXTreme Ten60Power™ .100" Pitch
Power/Signal Connectors
ET60X
ET60T / ET60S View Report
Q Strip® 0.80 mm Pitch High-Speed
Ground Plane Strips
QXE
QTE / QSE View Report
PowerStrip™/40 .250" Pitch
High-Power Strips
PEX
PET / PES Coming Soon!
Tiger Eye™ 1.27 mm Pitch
Micro Rugged System
Tiger Eye
SFM / TFM View Report
PowerStrip™/30 5.00 mm Pitch
Dual Blade Power Strips
Power Components
MPT / MPS Coming Soon!
FireFly™ Edge
Card Socket
FireFly
UEC5 Coming Soon!
Power Mate® .165" Pitch
Isolated Power Strips
IPBX
IPBT / IPBS Coming Soon!

CONTACT SALES

First Name
Last Name
Email
Company
Industry
Estimate Annual Usage
Family
Message

Don't want to fill out a form?
Chat with a product expert directly.

.
When researching women in electronics for a previous blog, I had way too much material to share. So here is a follow-on post that offers a summary of some interesting […] The post Women in Electronics: Technology Giants & Inventors appeared first on The Samtec Blog....
As we continue to work on a major overhaul to our navigation and back-end systems of the website, we were still able to make progress on a few key updates […] The post Here are the April 2024 Samtec Website Updates appeared first on The Samtec Blog....
Researching famous women in electronics led me in many directions and specialties, like mechanical engineering and computer science, and would easily turn this rather ambitious blog post into a book! […] The post Famous Women in Electronics appeared first on The Samtec Blog....
Designers frequently ask how much gold plating they should specify on the connector pins. As I write this blog, (and yes, I’m old-fashioned and am actually typing it; I’m not using […] The post Gold Plating On Connectors: How Much Do I Need? appeared first on The Samtec Blog....
Samtec Harrisburg attended the 17th annual Penn State Harrisburg Signal/Power Integrity Symposium and MASH Forum on Friday, April 19th 2024, hosted by the Center for Signal Integrity. The main goal of the […] The post Samtec Design Center Attends Annual Penn State Harrisburg SI/P...